Technical FAQs

Ask a Question

What specials are required on outdoor NEMA 3R duplex switches with REAR DOORS to meet UL requirements using the medium voltage metal enclosed product selector?

The outdoor duplex switches with REAR DOORS must be 80" deep and have full height vertical barriers behind each rear door. This is required because the duplex bus is located in the rear area.

CTA-ID : 2051466
Was this helpful?
What can we do to improve the information ?