Technical FAQs

Ask a Question

What is the minimum number of sections that can be ordered for outdoor (NEMA 3R) HVL/cc switchgear?

Two is the minimum number of sections. The base channels and roofs are 2 sections minimum. With special make parts a 20" wide single section can be created.


CTA-ID : 2051464
Was this helpful?
What can we do to improve the information ?