Technical FAQs

Ask a Question

I have two motors. What is the feasibility of using a 3 phase drum switch to run two different motors - one motor in one direction and the other motor in the other direction? I have part number 2601AW2. The voltage is 208V 3 phase.

We do not recommend running two motors with the drum switch due to internal wiring. Some wires are common to both sides.

CTA-ID : 2051273
Was this helpful?
What can we do to improve the information ?