Technical FAQs

Ask a Question

What are the repair parts for a QO14060M200RB, Series S02 (or S2) Load Center?

Issue:
Design repair parts

Product line:
QO load centers

Environment:
Repair parts

Cause:
Maintenance

Resolution:
Only the parts listed below are considered field replaceable.
Cover - 4056317450
Interior Trim with Labels - 4056313902K
Interior Assembly - QO14060M200RBI
Neutral Bonding Screw - 4028344850K
Main Circuit Breaker - QOM2200VH
Interior Trim Mounying Screw - 4020513001K
RB Door Mounting Screw - 2142217101
Outdoor Cover Latch - 4056314701
Outdoor Latch Rivet - 2410212160
Main Circuit Breaker and Main Lugs Keps Nut - 2342702001


CTA-ID : 2051233
Was this helpful?
What can we do to improve the information ?