Technical FAQs

Ask a Question

What is the main lug wire range for HCM23648?<br />

Four 3/0-750 kcmil Al/Cu is actual lug size; cable size per UL/CSA wire bending space is three 3/0-500 kcmil Al/Cu.


CTA-ID : 2050933
Was this helpful?
What can we do to improve the information ?