Technical FAQs

Ask a Question

Do offer a 100 Amp QO or Homeline ground fault circuit breaker?

Issue:
Do we have a QO or HOM 100 Amp GFI breaker?

Product Line:
QO-GFI, HOM-GFI

Environment: 
Minature Circuit Breakers

Cause:
Catalog selection

Resolution:
20A is the maximum single pole Homeline breaker with GFI that is available, and 50A is the maximum 2-pole Homeline breaker that is available.
30A is the maximum single pole QO breaker with GFI that is available, and 60A is the maximum 2-pole QO breaker with GFI that is available. Please note: the QO260GFI does not have a neutral connection it is suitable only for feeding 240 Vac and 208 Vac two-wire loads. 3-pole QO-GFI breakers are available up to 50A.
Was this helpful?
What can we do to improve the information ?