Technical FAQs

Ask a Question

What are the part numbers for the floats for the 9037DG`s and 9038JG`s.<br /><br />

For standard units with no special float forms, the 9037DG 1 through 3 uses 65073-003-50, the 4 through 8 uses 65073-003-51. The 9038 JG 1 through 5 uses 65073-003-51 and the 6,7, and 8 use two 65073-003-51.



CTA-ID : 2051257
Was this helpful?
What can we do to improve the information ?