Technical FAQs

Ask a Question

Does Square D offer a 3 phase, 225A sub-feed lug kit for QO load centers?

Issue:
Product Features

Product Line:
QO Load Center

Cause:
Product features

Resolution:
Three phase Sub-feed Lug kits for use in QO Load Centers are offered through 125A maximum. 


CTA-ID : 2051184
Was this helpful?
What can we do to improve the information ?