Technical FAQs

Ask a Question

What is the part number for the flexible cable mechanism for Powerpact H & J frame 2 & 3 pole circuit breakers?

9422CSF30 for 36 inch length
9422CSF50 for 60 inch length
9422CSF70 for 84 inch length
9422CSF10 for 120 inch length


CTA-ID : 2050935
Was this helpful?
What can we do to improve the information ?