Technical FAQs

Ask a Question

What is the deadfront part number for an HCN14524?

Issue:
Maintenance

Product Line:
Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 29 & 94-1989, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2000 IBC, 1995 NBCC 

Cause:
A dead front, also known as an "interior trim" may be misplaced or damaged when removed to service branch circuits in the panelboard.

Resolution:
The replacement deadfront is RPLHCN14524 or RPLHCN14524CU for copper interior





CTA-ID : 2051077
Was this helpful?
What can we do to improve the information ?