Technical FAQs

Ask a Question

Are the float accessories included with the 9038AW1 or 9038AR1 mechanical alternators?

No, Float accessories must be ordered separately. Type 9038AW1 and 9038AR1 must use center hole floats.
Center Hole Floats options are are listed as:
9049A6CS is a #304 stainless steel float , 5 feet stainless steel tubing and 4 stainless steel stops.
9049A6CA is a #304 stainless steel float, 5 feet aluminum tubing and 4 stops.
9049A6C is a #304 stainless steel float , 5 feet brass tubing and 4 brass stops
9049A6CS is a # 304 stainless steel float, 5 feet stainless steel tubing and 4 stops.




CTA-ID : 2051032
Was this helpful?
What can we do to improve the information ?