Technical FAQs

Ask a Question

Does the V3 switch door operator have a defeat mechanism for opening the door with the switch in the ON position?

No. Vario door operators are NOT defeatable. Suggest use the GS1 type for door defeating mechanism.


CTA-ID : 2050937
Was this helpful?
What can we do to improve the information ?