Technical FAQs

Ask a Question

Revision to resolution 2002855<br />Corrected answer to include the -F breakers.<br /><br />Do UL489 Multi 9 breakers have fingersafe terminals?

Fingersafe terminals are only available on ring tongue terminals of the UL489, 240Vac, Multi 9 breakers. Add an F suffix to the breaker part number to get the fingersafe version of the ring tongue terminals.

CTA-ID : 2051128
Was this helpful?
What can we do to improve the information ?