Technical FAQs

Ask a Question

Is there an alternate lug available for the DU326 safety switch?

Yes, but for current design, Series E03, only. Lug Kit GD4060LK, resticted to conductor combinations based on actual wire bending space provided in the switch, will provide terminals for (1) #1/0 AWG - 600 kcmil, (2) #1/0 AWG - 500 kcmil, or (4) #1/0 AWG - 250 kcmil, AL or CU conductors. The kit consists of (3) line lugs, (3) load lugs and (2) neutral lugs, as required for a 3-pole, 4-wire, General Duty switch.

CTA-ID : 2050411
Was this helpful?
What can we do to improve the information ?