Technical FAQs

Ask a Question

What is the replacement mushroom cap for the 9001 T mushroom operator?

NOTE- the following part numbers are for reference as they are all obsolete no longer available with no replacement.
For the plastic for the aluminum
1 3/8`` cap: 1 3/8`` cap :
black = 2358L906X1 3105204003
red = 2358L906X2 3105204002
green = 2358L906X5 3105204006
brown = 2358L906X4 3105204005
yellow = 2358L906X7 3105204008
orange = 2358L906X6 3105204007 blue = 2358L906X 3 3105204004



CTA-ID : 2050473
Was this helpful?
What can we do to improve the information ?