Technical FAQs

Ask a Question

Does the 9422ARP21 include a stainless steel handle?

The 9422ARP21 includes an A2 handle which is indended for use on stainless steel enclosures. All external parts are either stainless steel or chrome plated non-ferrous castings

CTA-ID : 2050574
Was this helpful?
What can we do to improve the information ?