Technical FAQs

Ask a Question

Should the CA4KN40BW3 come with a LED indicator.

Issue:
Should the CA4KN40BW3 come with a LED indicator.

Product Line:
Industrial Relays

Environment:
TeSys K IEC Style Relays

Cause:
Clarify if a LED light is still standard.                                                      

Resolution:                                                                 
LED indicators are no longer standard feature with relay. However, if LED indicator is needed customer could order separate suppressor module such as LA4KE1B.
 
Was this helpful?
What can we do to improve the information ?