Technical FAQs

Ask a Question

What components are used in an MHE360006F?

The MHE360006F consists of a MHL360006M molded case switch factory installed in a (modified) MA1000F enclosure. The enclosure markings are modified to indicate that the device is an enclosed molded case switch, not an enclosed circuit breaker.
NOTE: THE MA1000F, MA1000S, MA1000R, MA1000AWK AND MA1000DS ENCLOSURES ARE OBSOLETE AND NO LONGER AVAILABLE AS OF FEBRUARY, 2009.


CTA-ID : 2050428
Was this helpful?
What can we do to improve the information ?