Technical FAQs

Ask a Question

What Class of fuse does the D326N safety switch accept?

Issue:
Current class of fuse

Product Line:
General Duty Safety Switches

Environment:
Fuse classes

Cause:
Short Circuit current rating

Resolution:

This switch accepts Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit DRK600) and Class J fuses (current design Series E03 only - field install Class J Fuse Kit GDJK600). With Class H or K fuses installed, the switch is UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and DRK600 fuse kit installed) or Class J fuses (and GDJK600 fuse kit installed), the switch is UL listed for use on systems with up to 100,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 2050108
Was this helpful?
What can we do to improve the information ?