Technical FAQs

Ask a Question

What is the part number for the meters for a MMIAI or M5IAI ?

Issue:
Replacement ammeters

Product Line:
Medical Equipment

Environment:
Annunciators

Cause:
Parts for remotes

Resolution:
The parts had been  a 2ma meter = 6301002350 in the MMIAI and a 5ma meter = 6301060250 in the M5IAI . If the MMIAI is upgraded with a new LIM use a 5ma meter .  But these are now obsolete so use a remote.


CTA-ID : 2050200
Was this helpful?
What can we do to improve the information ?