Technical FAQs

Ask a Question

9007C - What type of plastic is the contact made from?<br /><br />

The case for our standard plug-in contact block (C54, C62, C68, etc.) is made of GE Valox 553. The cover is made of Dupont Zytel 70G-13-HS1-L. The remaining contact blocks (reed, compact, explosion proof) are all made of the Dupont Zytel 70G-13-HS1-L.



CTA-ID : 2049912
Was this helpful?
What can we do to improve the information ?