Technical FAQs

Ask a Question

Does Square D / Schneider Electric offer Manual Transfer Switches with provisions for circuit breakers as overcurrent protection in both directions?

Issue:
Selection

Product Line:
Manual Transfer Switches

Environment:
Availability

Cause:
Selection and ordering

Resolution:
Square D / Schneider Electric offers Fusible Manual Transfer Switches in 30, 60 and 100 Ampere, 240V and 600V, NEMA Type 1 and NEMA Type 3R ratings, but none with circuit breakers as the overcurrent protection.


 
Was this helpful?
What can we do to improve the information ?