Technical FAQs

Ask a Question

Will a QO14060L200G load center accept a QOT tandem or QO tandem circuit breaker?

This is a 40 space/60 circuit panel that will accept a maximum of 20 QOT (QOT prefix) tandem circuit breakers. QO tandem (QO prefix) are for use only in old-style (pre 1965) non-Class CTL panels. The QO tandem breaker should not be used in the subject load center.


CTA-ID : 2049962
Was this helpful?
What can we do to improve the information ?