Technical FAQs

Ask a Question

What is the length of the shaft for the door mounted rotary handle S36340 for the Powerpact H and J and NSF breakers?

Shaft length total is 18 13/16``
Square part of shaft is 18 1/8``
Dimension obtained by measurement.


CTA-ID : 2050222
Was this helpful?
What can we do to improve the information ?