Technical FAQs

Ask a Question

What is the torque value for the joint bolts for the ``busway joint connection`` on the obsolete SD type busway?

300 inch-pounds for the phase connections.
100 inch-pounds for the neutral ( if present ) connection.

CTA-ID : 2050306
Was this helpful?
What can we do to improve the information ?