Technical FAQs

Ask a Question

Can an LC series surge protector be used on a 240V circuit?

It is not rated for a 240V single phase circuit as found in the US. It is rated for the European 230V circuit, phase to neutral.

CTA-ID : 2050254
Was this helpful?
What can we do to improve the information ?