Technical FAQs

Ask a Question

Is ATS01 soft starter available in a NEMA 12 enclosure?

No, we don`t offer a NEMA 12 enclosure for this soft starter or any enclosure for it. Customer will have to use his own. Will have to use an ATS48 for NEMA 12 applications.

CTA-ID : 2050159
Was this helpful?
What can we do to improve the information ?