Technical FAQs

Ask a Question

Why are there no metal knockouts/ twistouts in the Interior breaker deadfront NFRPL430L2 . All the breaker spaces are empty/open

Issue:
Why are there no metal knockouts/ twistouts in the Interior breaker deadfront NFRPL430L2?

Product Line:
NF Pre-Series E1 (1997-2008) Panelboards

Environment:
Characteristic differences

Cause:
NF Series E1 evolution

Resolution:
All Series E1 NF breaker deadfronts (2008-Present) now require filler plates for the unused breaker spaces. The bag assembly is catalog number NFFP15, containing 15 single pole filler plates. You will have to order (2), to fill the entire 30 space section.


CTA-ID : 2049909
Was this helpful?
What can we do to improve the information ?