Technical FAQs

Ask a Question

What is the terminal lug data for the DGP36400E20LH main breaker provided in a CUM400CB, Series M01 Combination Service Entrance Device?

Issue:
Wire size range

Product Line:
Combination Service Entrance Device (CSED)

Environment:
Wiring components

Issue:
Needs to know the wire range of the breaker lugs

Resolution:
The load side lugs of the main breaker are suitable for use with (2) 2/0 - 350 KCMIL CU or (2) 2/0 - 500 KCMIL AL conductors per phase.



CTA-ID : 2050207
Was this helpful?
What can we do to improve the information ?