Technical FAQs

Ask a Question

What does the ``2`` mean at the end of a LC2K0601F72?

It is the addition of an integral coil supression device (bi-directional diode). Only available up to 240v


CTA-ID : 2049922
Was this helpful?
What can we do to improve the information ?