Technical FAQs

Ask a Question

What is the IP rating of Manual Motor Switch VCCF2?

It has an IP65 rating when using the gasket.


CTA-ID : 2049921
Was this helpful?
What can we do to improve the information ?