Technical FAQs

Ask a Question

What size is the horizontal ground bus?

As standard the ground bus is .25 x 1.5 which is 300 amp, we have a selectable offering for 600 amp which is .25 x 2.


CTA-ID : 2049863
Was this helpful?
What can we do to improve the information ?