Technical FAQs

Ask a Question

What is the shaft size for the 9007 limit switch?<br /><br />

Our 9007 C`s are 3/8`` shaft; Y247 is 5/16``; and the type T , TF are 3/4``.



CTA-ID : 2050059
Was this helpful?
What can we do to improve the information ?