Technical FAQs

Ask a Question

Is MSC mounting base copper or aluminum? What is the interrupting rating?

Rating is 10 kA for 0.05 seconds.
Bus material is tin-plated copper.


CTA-ID : 2049994
Was this helpful?
What can we do to improve the information ?