Technical FAQs

Ask a Question

What are the box lug wire sizes for the UL 489 Multi9 breaker breakers?

The .5A thru 25A breaker have a wire range from #18 AWG to #4 AWG; the breakers rated from 30A to 35A have a wire range from #18 AWG to #2 AWG.


CTA-ID : 2050043
Was this helpful?
What can we do to improve the information ?