Technical FAQs

Ask a Question

What is the limiting factor in the number of comb bus bars to be used with an interconnected row of GV2 starters ?

Make sure the total amperage load of starter devices does not exceed 63 amps ( ie. 3 or 4 or 5 bus bars could be tied together if the loading only totalled 55a ) .


CTA-ID : 2049998
Was this helpful?
What can we do to improve the information ?