Technical FAQs

Ask a Question

Is the NS400H circuit breaker 100% rated?

The NS400H is an IEC rated breaker, so the 100%/80% rule does not apply. The breaker is not UL rated. It can be loaded up to 100% of its value without regard to number of hours it is in service.


CTA-ID : 2049977
Was this helpful?
What can we do to improve the information ?