Technical FAQs

Ask a Question

Will the 60 circuit HOMELINE load centers accept a HOMT tandem or quad circuit breaker?

The 60 circuit HOMELINE load center is a 40 space/60 circuit panel that will accept a maximum of 20 HOMT tandem or 10 HOMT quad circuit breakers.


CTA-ID : 2049975
Was this helpful?
What can we do to improve the information ?