Technical FAQs

Ask a Question

Can 300A vertical bus be replaced with 600A vertical bus?

No, it is not a direct replacement.
It can be replaced but requires a 600A vertical bus shroud also.


CTA-ID : 2050035
Was this helpful?
What can we do to improve the information ?