Technical FAQs

Ask a Question

Can the shaft of the LU9AP00 Through-the-Door Operating Mechanism for the U-Line Starter be cut so that it will fit into an enclosure that is less than 7.5 inches deep?

No, the LU9AP00 can`t be go into a less than 7.5 inch deep enclosure.

CTA-ID : 2050016
Was this helpful?
What can we do to improve the information ?