Technical FAQs

Ask a Question

Does the jumper on T1 and T2 on the terminal strip of a PGL breaker need to be removed if wired with a neutral CT?

Yes. Remove and discard the shorting jumper from T1 and T2, if a CT is installed. The installation guide for that trip unit is: 48041-082-03.


CTA-ID : 2049902
Was this helpful?
What can we do to improve the information ?