Technical FAQs

Ask a Question

Is the main breaker included with an 800A OEM I-Line interior, catalog number HMA675S8?<br />

These OEM interiors do not come with a main breaker, they are continuous bus interiors. If a main breaker is needed, it can be backfed on the bus.

CTA-ID : 2050320
Was this helpful?
What can we do to improve the information ?