Technical FAQs

Ask a Question

What is the solid neutral assembly for a P1200R, P1200S, or P1200AWK circuit breaker enclosure?

Issue:
What is the solid neutral assembly for a P1200R, P1200S, or P1200AWK circuit breaker enclosure?

Product Line:
Powerpact P-frame enclosures

Environment:
Molded Case Circuit Breakers

Cause:
Accessories

Resolution:
If the P-frame Powerpact breaker being used is not provided with integral ground fault protection, use neutral assembly SN1200. If the P-frame Powerpact breaker being used does have integral ground fault (suffix U44*, U64* or U74*), use neutral assembly S33576MK and order the Neutral CT S33576 separately.
Was this helpful?
What can we do to improve the information ?