Technical FAQs

Ask a Question

Is the JD250S UL Listed or CSA Certified?

The JD250S is cULus Listed, File E-136861. This listing should be acceptable in Canada.


CTA-ID : 2050783
Was this helpful?
What can we do to improve the information ?