Technical FAQs

Ask a Question

What type primary fuses are used in MCC starter units with control transformers? <br />What is the part number?

Primary fuses are FNQ-R type fuses
480V 50VA CPT- .25 amp 25430-20025
480V 100VA CPT- .5 amp 25430-20050
480V 150VA CPT- 1.0 amp 25430-20100
480V 300VA CPT- 1.6 amp 25430-20161
480V 500VA CPT- 2.8 amp 25430-20281

CTA-ID : 2050133
Was this helpful?
What can we do to improve the information ?