Technical FAQs

Ask a Question

Does the ATV31 drives meet the European EMC directives?

The 230VAC single phase input (M2) and the 460VAC three phase input (N4) drives meet EN5501 Class A EMC requirements because there is an internal EMC filter.
The 3 phase single phase in units (M3X) do not have this internal filter.
To meet EN 55022 Class B requirements you must use the external EMC filter.

CTA-ID : 2050360
Was this helpful?
What can we do to improve the information ?