Technical FAQs

Ask a Question

What Class of fuse does the D326NTR safety switch accept?

This switch accepts 300Vac, Class T fuses only. With Class T fuses installed, the switch is UL listed for use on systems with up to 100,000 RMS Symmetrical Amperes available fault current.


CTA-ID : 2050110
Was this helpful?
What can we do to improve the information ?