Technical FAQs

Ask a Question

What is the part number for the replacement mushroom knob for a 9001T operator?

Note - The Type T devices are obsolete. A number of these knobs are obsolete no longer available with no replacement. They will all be obsolete soon. Check system for availability.

1 3/8 inch diameter 2 1/4 inch diameter
Red 2358C6G2 Red 2358C22G2
Black 2358C6G3 Black 2358C22G3
Green 2358C6G6 Green 2358C22G6
Orange 2358C6G7 Yellow 2358C22G8
Yellow 2358C6G8

CTA-ID : 2050472
Was this helpful?
What can we do to improve the information ?