Technical FAQs

Ask a Question

Does the catalog number AL250KA lug kit include the bolt that mounts the lug through the back of the breaker?

The mounting bolt is included with the AL250KA kit. The mounting bolt/screw is not available as a separate catalog number.

CTA-ID : 2050072
Was this helpful?
What can we do to improve the information ?