Technical FAQs

Ask a Question

What is the Square D part number for a lug equivalent to ILSCO part number D3121 or CMC part number LA750-2 ?

Issue:
Cross Reference

Product Line:
Safety Switch

Cause:
Lug cross reference

Resolution:
Square D part number 40251-136-50 is the lug that we purchase from ILSCO (same as D3121) and CMC (same as LA750-2).


CTA-ID : 2050012
Was this helpful?
What can we do to improve the information ?